{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How tall is the NetShelter WX with the optional castor kit attached?
Issue:
Customers may ask for the total height of the NetShelter WX with the optional castor kit attached.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
Cabinets that are floor mounted may have height restrictions.

Resolution:
The NetShelter WX with the optional castor kit attached is approximately 731 mm (28.78") tall.

Schneider Electric Egypt and North East Africa