{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
KBB40ZFGU What the possible diameter of the pipes / cables acceptable in the clips
This Cable bracket KBB40ZFGU can be used to fix additional tubes or cables to KBA or KBB. It is delivered with 3 fixed clips, 13mm internal diameter + 2 lateral clip (not installed, but delivered with the kit) designed for clipping 16mm
The device Also have 2 lateral fixation for customer custom plates Max thickness 4mm, who should have 2 square holes, 4mm (distance 42 mm)

Schneider Electric Egypt and North East Africa

Attachment(s)
KBB40ZFGU.JPG.jpg [17.33 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.