Search FAQs
Can you order the ATV212 or SFD212 drives with a Bacnet option card?
Issue:
Ordering an ATV212 or SFD212 with Bacnet option card.
Product Line:
ATV212 or SFD212
Environment:
All
Cause:
Wants to order the ATV212 or SFD212 drive with a Bacnet option card.
Resolution:
Yes Bacnet is standard on the ATV212 and SFD212 drive.
Ordering an ATV212 or SFD212 with Bacnet option card.
Product Line:
ATV212 or SFD212
Environment:
All
Cause:
Wants to order the ATV212 or SFD212 drive with a Bacnet option card.
Resolution:
Yes Bacnet is standard on the ATV212 and SFD212 drive.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: