{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the purpose of the external battery of the M221?
1) The help content give us the information the battery of the M221 allow:
-to save the content of the whole %MW area ( %MWi  with i>50;  note: %MW0-%MW49 are also save without battery)
- to save the RTC clock

2) But in reality the battery is always needed/mandatory because without battery the PLC can’t start in RUN after a PowerOFF, PowerON of the PLC
Within %S75 the PLC program can check when the battery has the be replaced before it become out of order  (in average every 4/5 years):

When this bit is Set to 1, it means external battery power is low, so has to be replaced soon

Schneider Electric Egypt and North East Africa

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.