{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the part numbers of the measuring board for ATV61HC16N4 and ATV71HC13N4 drives?

Issue:
Needs the part numbers of the measuring board for the ATV61HC16N4 and ATV71HC13N4 drives

Product Line:
ATV61 and ATV71

Environment:
All

Cause:
Failed measuring board component within the drive.

Resolution:
The part number for the measuring board is VX5A71HC13N4 or VX5A71HC13N4F (For Fuji parts)
When a replacement Measurement board is needed, the serial  number of the VFD needs to be verified.

If the 8th digit of the Serial number is a "2" as shown below than the replacement part number must have an "F" suffix.
See Attachment

Schneider Electric Egypt and North East Africa

Attachment(s)
Fuji.png [10.72 KB]