Issue:
What is the MTBF on the BMXNOR0200H?
Product Line:
BMXNOR0200H
Resolution:
What is the MTBF on the BMXNOR0200H?
Product Line:
BMXNOR0200H
Resolution:
Product | Mtbf 30° Continuous | Mtbf 30° Intermittent | Mtbf 60° Continuous | Mtbf 60° Intermittent | Mtbf 85° Continuous | Mtbf 85° Intermittent | Nb Cpt Missing | Nb Cpt Missing * Qty | Nb Cpt Total * Qty | Ratio Nb Cpt Missing / Nb Cpt Total |
BMXNOR0200H | 568910.735 | 466220.897 | 438931.658 | 374348.166 | 311442.943 | 278618.975 | 9 | 14 | 497 | 2.80% |
Released for:Schneider Electric Egypt and North East Africa