{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there documentation available that shows the rackmount depths for Dell products?

Issue:
Some Dell products have mounting rails that interfere with a PDU, or mount so deep that the rear doors won't shut.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Some Dell products extend beyond the rear mounting rails of the cabinet, and also have cable management that intrudes even further into the rear of the cabinet.

Resolution:
The attached file is a web page from Dell that shows many Dell rackmount products, optional rail kits and their optional cable arms. This document shows the overall mounting depths of these various rail kits and their options. There is also a section that has other notes regarding compatibility of these rail kits, specific to the NetShelter SX 600mm W x 1070mm D cabinets.
This document was found at: http://i.dell.com/sites/content/business/solutions/engineering-docs/en/Documents/rail-rack-matrix.pdf
See attached file.

Schneider Electric Egypt and North East Africa

Attachment(s)

Dell Enterprise Systems Rail Sizing and Rack Compatibility Matrix.pdfDell Enterprise Systems Rail Sizing and Rack Compatibility Matrix.pdf [3.21 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: