{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find information on the fault codes for the ATV21/212 drive?

Issue:
Fault Code Information for the ATV12/212 Drives.

Product Line:
ATV21
Altivar 21
ATV212
Altivar 212
S-Flex

Environment:
All serial numbers for ATV21/212 Drives

Cause:
N/A

Resolution:
Information for the ATV21/212 drive can be found in the programming manual for the drive.

ATV21 Programming Manual is available for download here: https://www.se.com/ww/en/download/document/AAV75193/
ATV212 Programming Manual is available for download here: https://www.se.com/ww/en/download/document/S1A53838/

Schneider Electric Egypt and North East Africa