{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Trend Summary Report line graph omitting devices
Issue
A Trend Summary report is run that includes multiple devices. The line graph that is included in the report will show 2+ devices but not all of the devices.  At the same time, all of the devices are listed below the line graph in the trend summary chart.

Trend Summary Report

Product Line

Power Monitoring Expert 7.2.x

Environment
Web Applications "Reports"
Causes
The Load Profile report assumes a standard logged interval of data for all included devices. If there are devices that are being logged at varying intervals it will pick devices that are logging at the same interval and exclude the others.

Resolution
The solution is to make sure all of the devices are logging at the same interval. eg. All KW demand readings will log every 15 minutes

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: