{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What will cause the ATV212 not to go into local mode when pressing the LOC/REM button?

Article available in these languages: Spanish


Issue:
What will cause the ATV212 not to go into local mode when pressing the LOC/REM button?

Product Line:
ALTIVAR 212, ALTIVAR 21

Environment:
All serial number

Cause:
When pressing the LOC/REM button the drive will not go to LOC mode.

Resolution:
This could possibly be due to parameter F732 (LOC/REM button disabled) being set to 1. If so, set F732 to 0.   However, if the LOC/REM button is not disabled, then it is likely, the keypad is defective, the drive will need to be replaced.

Schneider Electric Egypt and North East Africa