{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the 8903L, 8903LX, and 8903S Square D lighting contactors rated for LED lighting applications?
Issue:
Documentation for LED lighting loads or ratings for 8903L or 8903LX lighting contactors?

Product Line:
Class 8903 Type L/LX Lighting Contactors

Environment:
NEMA Lighting Contactors

Cause:
Application information

Resolution:

As of 2017 Schneider Electric has tested the Class 8903 Type L/LX and Type S NEMA lighting contactors per NEMA-410-2015 and UL508: Table 46.1 and Section 61C.
(Test procedures for LED Loads).

This test specifies procedures up to 16A loads at 120VAC. Our testing was performed at 20 amps 120VAC and passed all of the requirements

Schneider Electric Egypt and North East Africa