{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Advance One Line Crashing with error "Password Encryption Failed - Cipher initialization failed" in the AdvanceOneLine Status log
Issue
Advance One Line crashes without any errors. However, there is an error in the advance one line Status log, which read "Password Encryption Failed - Cipher initialization failed"

Product Line

Powerlogic Scada 7.40

Environment
Starting runtime, and advance one line in PLScada

Cause
Running the Computer configuration multiple times and clicking on the "Register".

Resolution

Solution 1

- Go to C:\ProgramData\Schneider Electric\PowerSCADA Expert\v7.40\User
- Go to the folder with the project name in use
- Open the advoneline.ini file with Notepad
- Delete the entries and leave only the first line
- Restart Advance One Line

Solution 2
- Go to C:\ProgramData\Schneider Electric\PowerSCADA Expert\v7.40\Config
- Rename PowerLogic.Cipher.dll.confg to PowerLogic.Cipher_old.dll.
- Restart Advance One Line

Renaming PowerLogic.Cipher.dll. forced it to regenerate the key for the machine






Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.