{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you program the ATV212 Drive to do an automatic restart after power loss in local control?
Issue:
ATV212 configuration to do an automatic restart after power loss in local control

Product Line:
Altivar ATV212

Environment:
All

Cause:
Running the drive in local mode they need to have the drive restart in the event of loss of power.

Resolution:
The drive can not be programmed to do a automatic restart in local mode. You will need to push the start button again on the face of the drive to start the drive back up.
If you want a automatic restart after power loss consider using 2 wire terminal control instead.

Schneider Electric Egypt and North East Africa