{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the VW3A3310 and the VW3A3310D Modbus Ethernet TCP/IP option cards?
Issue:
VW3A3310 with a "D" on the end of the part number.

Product Line:
ATV71 and ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
The "D" on the end of the VW3A3310D indicates it is equipped for daisy chain and has dual RJ45 connectors.  A network cable can go into one RJ45 and out the other to connect to the next drive in the network.  The VW3A3310 has only one RJ45 port.

Schneider Electric Egypt and North East Africa