{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Pin-out for VX003 PC cable for RS232 port of VAMP 200 series

Issue:
Trying to connect to the VAMP 200 series through the RS232 port fails.

Product Line:
VAMP 255, VAMP 257,  VAMP 259, VAMP 200 series, VX003

Environment:
Connecting to VAMP set to configure settings.

Cause:
The RS232 port configuration is not a standard RS232 port.

Resolution:
Image 1

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: