{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is a fault code cleared or reset, on ATS22?
Issue:
Needs to clear a fault code, on the ATS22 soft start.

Product Line:
Altistart 22

Environment:
All models

Cause:
The fault code must be cleared to make ATS22 functional.

Resolution:
After the condition that created the fault has been corrected, a fault reset can be accomplished several ways:

1) Remove control power from CL1-CL2. After the display has gone blank, apply control power.
2) On the integral or remote keypad, press the 3-key combination of ENT / UP arrow / DOWN arrow, simultaneously.
3) Wire a reset contact to logic input LI2 or LI3 and program it to rSt (remote reset). A momentary contact closure will reset.
4) Use Modbus command word 752 and write a 1 to bit 3

Note that several fault codes require method 1) above.  These are InF, trAP, SCF.

Schneider Electric Egypt and North East Africa