Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What are the conditions for closing the ATS48 R2 relay?
Issue:
ATS48 R2 relay closing conditions

Product Line:
Altistart 48

Environment:
All models

Cause:
None

Resolution:
The R2 relay is an End of Starting relay. It has a dedicated function to control a shorting contactor. It is not programmable.
The relay contact is normally open and will close when the motor is up to full speed.
The conditions for R2 closure are:
- If CLP = OFF, relay closes when the thyristors are full wave (angle = 1), full voltage is being sent to the motor.
- If CLP = ON, relay closes when the thyristors are full wave (angle = 1) and the peak current estimated is less than 1.4 x In.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: