{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION7650/7550 - Communications to Optical Port (COM4) are Unsuccessful
Issue:
Serial settings have been changed on the COM4 Optical port on an ION7650/7550. Settings have been confirmed on the software and PC side of the optical probe, yet communications cannot be established.

Product Line:
ION7650/7550

Environment:
ION7650/7550 Optical Communications

Cause:
On firmware versions other than the latest (v. 373), certain optical port settings are not actually changed even though the change appears to have taken place on both the front panel and in ION Setup.

Resolution:
Upgrade the meter to the latest firmware (v. 373). A temporary solution is to power cycle the meter which will apply the serial settings and allow communication to COM4.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.