{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What data types are supported by the Real Time Tables in PME and SPM?
Issue:
There are measurements available on a device such as a device's serial number and volts mode. However these measurements are not available for selection in the real time tables

Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0

Environment:
Web Applications Real Time Tables

Cause:
Real Time Tables support only certain data types. The measurements that do not appear in the list of available measurements are of a type that is not supported.

Resolution:
Real Time Tables only supports the following data types: numeric, date, boolean.

String type such as device type, serial number and volts mode cannot be displayed.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: