{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the THD (Total Harmonic Distortion) for the 140ACI03000 module?

We only specify THD for discrete AC input modules. The 140ACI03000 is strictly 1-5VDC or 4-20mA.

This card has no additional filtering capability outside of the built in low pass filter (-3db cutoff @ 15Hz, +-20%).

If the signal is simply too noisy and can not be cleaned up before it gets to the module, you can try creating some sampling or averaging logic.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: