Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Error: "Request ExecuteCipher fail at function call;ConfigureCipher" during Powerlogic Scada installation
Issue
Customer gets an error during the installation that reads Request ExecuteCipher fail at function call;ConfigureCipher"



Product Line 
Powerlogic Scada 7.40

Cause 
 Powerlogic Scada was installed in the machine preciously and the uninstall did not get rid of all the registry files. This could be either the same version, or an older version. 

Resolution
Download the attachment and run the .bat file on server where Powerlogic Scada needs to be installed. Try to install the software again after running the .bat File

 

Schneider Electric Egypt and North East Africa

Attachment(s)
UninstallPSE_7.40.bat [1.79 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: