{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Unity takes too long to download an application containing a large amount of DTM's through the NOE
Issue
Unity takes too long to download an application containing a large amount of DTM's  through the NOE.

Product Line
Unity

Environment
Windows 10, windows 8, Windows 7

Resolution
If the Unity application contains a large number of DTM's, downloading the application using the '140NOE771xx'  module can
take upto 10 minutes on a Pentium dual core PC.  This can occur if applicatiion is huge and there is not enough bandwidth
on the NOE module or the PC does not meet the requirements for running Unity.

The download time can be reduced by using the following options
  • Ensuring that the PC meets the requirements defined in the 'Readme.html' on the Unity CD.
  • Using a faster PC.
  • Adjusting the 'Maximum Unity data exchange by PLC scan' parameter in the PLC configuration (Only If the PC meets the requirements.).
wffw


Schneider Electric Egypt and North East Africa