{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I use the concatenate script in Vijeo Designer to join two strings variables?
Issue:
How do I use the concatenate script in Vijeo Designer to join two strings variables?

Product Line:
Vijeo Designer

Resolution:
Below is a sample script that will concatenate two strings into a single string variable.
NOTE: MyString1, MyString2, Combined_String are variables that are external from the script defined in the Vijeo Designer Navigator -> Target01 -> Variables node.
String string1_temp, string2_temp, combine_temp;    // internal script variables defined here

string1_temp = MyString1.getStringValue();        // let string1_temp equal to MyString1
string2_temp = MyString2.getStringValue();        // let string2_temp equal to MyString2

combine_temp = string1_temp1.concat(string1_temp2);    // concatentate string1_temp with string2_temp and let it equal to combine_temp

Combined_String.write(combine_temp);        //write the concatentated string into an external variable called Combined_String

Schneider Electric Egypt and North East Africa