{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an ION7330/7350 framework be added to a PM8000 meter
Issue
Can an ION7330/7350 framework be added to a PM8000 meter

Product Line
PM8000 series

Environment
ION Setup, StruxureWare Power Monitoring Expert Designer

Cause
A user wants to copy a framework from an ION7330 meter to PM8000 meter.

Resolution
The default ION73x0 framework will not work in the PM8000. The PM8000 has added some ION modules, as well as removed certain modules (modules removed because new, enhanced modules replaced them). Customized pieces of framework can be added to the PM8000 meter provided the modules are supported on the PM8000. Refer to the IONDeviceTemplateReference for a list of supported modules in the PM8000.

Schneider Electric Egypt and North East Africa