{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I associate a custom alarm sound for new alarms in PME?
Issue:
Customer would prefer to play a different sound when there is a new alarm in Power Monitoring Expert

Product Line:
Power Monitoring Expert 7.2.x

Environment:
Power Monitoring Expert Software Configuration

Cause:
The default sound for a new alarm may not be something the customer wants to listen to when they get a new alarm.

Resolution:
Navigate to the Power Monitoring Expert folder. Inside the system/etc folder there is an alarm.wav file. Replace that with the desired .wav file of your choice, Please note that the desired .wav file must be named alarm.wav or it will not play as desired, and this will be the new alarm that plays.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.