{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which parts of a NetShelter cabinet are considered user replaceable?
Issue:
Need to determine which NetShelter components can be replaced by customers in the field.

Product Line:
NetShelter SX, SV, VX

Environment:
All versions and serial ranges.

Cause:
A part of the cabinet has been damaged and needs to be replaced.

Resolution:

Many parts of the cabinet are designed to be user replaceable: roof, side panels and doors.
The user manuals show how to replace these parts. The manuals are available on the APC website.
  • The roof can be removed by disengaging two hinge pins, then they simply lift off. NOTE: The NetShelter SV roof is not removable.
  • The sides can be removed by unlocking them, then they simply lift off.
  • The doors can be removed by disconnecting the ground wire, then they simply lift off.
If cabinet parts are damaged in transit by a Schneider Electric carrier (Shipped from Schneider Electric, Freight Prepaid & Add) we will send user replaceable parts-only free of charge. Installation is not included.

Schneider Electric Egypt and North East Africa