{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
ATV212 or S-flex drive is running full speed with PID enabled drive does not appear to be responding to the PID feedback.
Issue:
ATV212 or S-flex drive is PID does not appear to be responding to the PID feedback.

Product Line:
Altivar ATV212 S-flex

Environment:
All

Cause:
Drive is running full speed and is not responding to the PID feedback

Resolution:
Troubleshooting Tips:  Check the PID feedback signal 1st to see if the drive is getting good feedback.
Check the programming F360 make sure its set to the PID feedbacks input.  VIA-1 or VIB-= 2
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.