{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to import SoMachine/Machine Expert - Basic symbols in Vijeo Designer?
Using SoMachine Basic in SoMachine Central
  1. First you need to export your project as "SoMachine Basic project" (see attachment 1)
  2. Second in Vijeo designer:
  • Add in the IO Manager a Modbus TCP/IP  Drive and select Modbus Equipment
  • Write the IP Address of the M221 PLC and check the case IEC61131. Also you need to select the Double word order. (see attachment 2)
  • Do a right click in the "Variables”, select "Link Variables", select type files "*.SMPB" and then select your project (see attachment 3)
  • Now you can select witch symbols do you want to import

Using SoMachine/Machine Expert - Basic standalone

In Vijeo designer:
  • Add in the IO Manager a Modbus TCP/IP  Drive and select Modbus Equipment
  • Write the IP Address of the M221 PLC and check the case IEC61131. Also you need to select the Double word order. (see attachment 2)
  • Do a right click in the "Variables”, select "Link Variables", select type files "*.SMPB" and then select your project (see attachment 3)
  • Now you can select witch symbols do you want to import







Schneider Electric Egypt and North East Africa

Attachment(s)
3.png [83.66 KB]
1.png [103.01 KB]
2.png [80.04 KB]