NVLs (global network variables) will work in the Ethernet port 2 of the M251 only if the Ethernet port 1 status is "Data Exchange".
Ethernet port 1 is in "Data Exchange" when the ethernet cable is connected and the PLC has a valid IP address.
Note: You can check the status of the ETH port 1 using the system variable PLC_GVL.ETH_R.i_wPortALinkStatus.
Ethernet port 1 is in "Data Exchange" when the ethernet cable is connected and the PLC has a valid IP address.
Note: You can check the status of the ETH port 1 using the system variable PLC_GVL.ETH_R.i_wPortALinkStatus.
Released for:Schneider Electric Egypt and North East Africa