Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the main causes of the Fault: [SCF] - Short Circuit Fault for VFD?
The SCF fault can happen due to below reasons, 
 
1. Short-circuit or grounding at the drive output due to motor or cable short circuit, cable damage etc... 
2. Significant Ground Leakage current at the drive output if several motors are connected in parallel. 
3. The drive IGBT short circuit (drive failure) 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: