Search FAQs
Routing register for L9_MSTR control block with M340 native ethernet port
Title
Routing register for L9_MSTR function
Issue
L9_MSTR function block usage
Product Line
M340
Environment
Unity Pro, Control expert
Resolution
Unity Pro LL984:
After completing a conversion of a LL984 project from ModSoft,, ProWrox or Concept to Unity Pro the new L9_MSTR function block needs to be modified to operate properly with an M340 CPU native ethernet port. The high byte or MSB of the 4th implied word in the control array must be set to address 254 or 16#FE in order for the block to communicate out from the M340 native ethernet port.
Routing register for L9_MSTR function
Issue
L9_MSTR function block usage
Product Line
M340
Environment
Unity Pro, Control expert
Resolution
Unity Pro LL984:
After completing a conversion of a LL984 project from ModSoft,, ProWrox or Concept to Unity Pro the new L9_MSTR function block needs to be modified to operate properly with an M340 CPU native ethernet port. The high byte or MSB of the 4th implied word in the control array must be set to address 254 or 16#FE in order for the block to communicate out from the M340 native ethernet port.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: