{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up the VW3A1101 keypad so that you can use the keypad to program the drive?
Issue:
VW3A1101 keypad set up to program the drive

Product Line:
Altivar 61, 71, 312, 212

Environment:
All

Cause:
VW3A1101 usage with drives.

Resolution:
You will need to set up the access level to advanced in the Main Menu.  This will give you access to most of the drives set up parameter settings in the HMI.
For assistance see the complete drives ATV61 programming manual.

Schneider Electric Egypt and North East Africa

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]