Search FAQs
Video: How are the R1, R2, and R3 relays programmed on the Altivar Process Drives?
Issue:
Relays configuration on the Altivar Process Drives
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All products of ATV630
Cause:
Relay program assignment
Resolution:
Under the MAIN MENU, select Menu 5 COMPLETE SETTINGS.
Scroll down to [INPUTS/OUTPUTS], Press F4 key to go to [RELAY] and select [R1 CONFIGURATION] r1.
Select R1 Assignment and then select the desired function, such as No drive flt, Drv running, etc...
The same can be done for [R2 CONFIGURATION].
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: