{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV312 require separate 120V control voltage to run the drive?
Issue:
Separate 120V control voltage needed to run an ATV312?

Product Line:
ATV312

Environment:
All

Cause:
Customer does not have 120VAC available

Resolution:
No.  A separate 120Vac is not needed.  Only line voltage is required.
When remote control is used, the VFD provides 24Vdc for the logic inputs.

Schneider Electric Egypt and North East Africa