{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why won't my Smart-UPS RT go to bypass in 240v environment

Issue:

Smart-UPS RT will not go to bypass with 240v input and 208v output

Product Line:

Smart-UPS Online

Environment:

All models, All Serial Numbers

Cause:

Smart-UPS RT units will not go to bypass if the input voltage is out of range. By default the UPS is configured to output 208v. If you are feeding the UPS 240v, the input may be outside of the acceptable range for bypass. In this situation you should configure the UPS to also output 240v. You are able to configure the acceptable range for bypass operation and UPS output voltage via the Network Management Card. Please note that the UPS output power must be turned off in order to make this change.

Resolution:

Ensure that UPS output is set to match UPS input in order to ensure proper bypass operation. Adjust Bypass voltage thresholds as needed.

Schneider Electric Egypt and North East Africa