{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Total Power Off Procedure for All Single Phase Symmetra Units

Article available in these languages: Russian

Issue
Proper procedure for powering down a single phase Symmetra

Product Line
Symmetra LX, Symmetra RM, Symmetra Power Array

Environment
All Single Phase Symmetra

Cause/Overview
There are times when it may be required to power down the Symmetra. Such instances could be to change out a system fan depending on the type of Symmetra, or changing out a backplate.

Resolution
The total power off procedure for Symmetra systems are found on the back of all of the systems.
The procedure is as follows:

1. Set the System enable Switch to Standby
2. Set the Input Circuit Breaker to Standby
3. Disconnect the Battery Modules
4. Disconnect external Battery Cabinet (if provided)
5. Disconnect Mains/Branch Circuit




Schneider Electric Egypt and North East Africa