Issue
How to determine the IP address of ION 7550 RTU with no display within a given range of IP addresses
Product
ION 7550 RTU with no display
Environment
Networking
Resolution
Use nmap to scan an IP address range and return the mac address found. ION7550 RTU meters will have a MAC address that starts with 00:60:78
1) Download nmap from https://nmap.org/
2) In command prompt navigate to the folder where nmap.org is located (eg. cd "c:\Downloaded\nmap")
3) Run the command nmap -p 23,80,502,7700 [Ip address range] (eg. nmap -p 23,80,502,7700 10.10.1.100-150)
4) Examine the results and determine IP address of device(s) with Mac Address 00:60:78. Below is an example of the results
Nmap scan report for 10.10.1.107
Host is up (0.00s latency).
PORT STATE SERVICE
23/tcp open telnet
80/tcp open http
502/tcp open mbap
7700/tcp open unknown
MAC Address: 00:60:78:64:32:14 (Power Measurement)
5) Connect to the web page with the specific IP address found in Step 4 to verify the serial number or owner/tag information
Released for: Schneider Electric Egypt and North East Africa