Search FAQs
Can I get the Magelis HMI to communicate to the Unity Pro Simulator?
Issue
Can I get a Magelis or Harmony HMI to communicate to the Unity Pro or EcoStruxure Control Expert Simulator?
Product Line
Harmony / Magelis XBTGC/GH/GK/GT, HMIGTO/GTU/STO/STU, iPCs, Panel PC, Box PC, Unity Pro, EcoStruxure Control Expert
Environment
Physical HMI Communication with Simulated PLC
Resolution
Yes, it is possible for the Harmony or Magelis HMI communicate to an EcoStruxure Control Expert or Unity Pro simulator. Make sure in the Modbus/TCP driver in Vijeo Designer is used. The IP address of the Equipment is the IP address of the PC that is running the EcoStruxure Control Expert or Unity Pro Simulator. The PC will need to open TCP Port 502.
If the Vijeo Designer Simulation is on the same PC as the PLC Simulation, the IP Address needed is 127.0.0.1 (the local host).
Can I get a Magelis or Harmony HMI to communicate to the Unity Pro or EcoStruxure Control Expert Simulator?
Product Line
Harmony / Magelis XBTGC/GH/GK/GT, HMIGTO/GTU/STO/STU, iPCs, Panel PC, Box PC, Unity Pro, EcoStruxure Control Expert
Environment
Physical HMI Communication with Simulated PLC
Resolution
Yes, it is possible for the Harmony or Magelis HMI communicate to an EcoStruxure Control Expert or Unity Pro simulator. Make sure in the Modbus/TCP driver in Vijeo Designer is used. The IP address of the Equipment is the IP address of the PC that is running the EcoStruxure Control Expert or Unity Pro Simulator. The PC will need to open TCP Port 502.
If the Vijeo Designer Simulation is on the same PC as the PLC Simulation, the IP Address needed is 127.0.0.1 (the local host).
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: