Search FAQs
What is the difference between the config\translators and config\templates folders
Issue:
In the Power Monitoring Expert config folder, there are two folders called "translators" and "templates". Driver files created in the Modbus Device Importer (MDI) may appear in one or both of the folders but it is not clear what each folder is used for.
Product Line:
ION Enterprise
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment:
Windows Explorer
Modbus Device Importer
Resolution:
Power Monitoring Expert uses the config\translators folder for its custom device drivers. Only files in this folder will be used by the software. The config\templates folder is essentially a staging area for driver development until they are ready to be applied to the system. When drivers are created using the Modbus Device Importer, the program will default to the config\templates folder to save the .ion and .xml files (although the files can be saved in any location). When "Add Device Type" or "Update Device Type" is selected in the Modbus Device Importer, the driver files are then copied into the config\translators and are ready for use. There will now be two sets of the same driver files, one in the config\templates folder and the other in the config\translators.
At this point, it is possible to modify either set of files. If the files in the config\templates folder are opened in the Modbus Device Importer and modified, those changes will automatically be copied to the files in the config\translators folder upon selecting "Update Device Type".
Note: In Power Monitoring Expert 9.0, the Device Type Editor has been added as a replacement for the Modbus Device Importer. Using the DTE to modify drivers in the config\translators folder will result in a "file in use" error when attempting to install the driver. Therefore the files in the config\templates must be modified and any changes will then be applied to the config\translators files when the driver is installed.
In the Power Monitoring Expert config folder, there are two folders called "translators" and "templates". Driver files created in the Modbus Device Importer (MDI) may appear in one or both of the folders but it is not clear what each folder is used for.
Product Line:
ION Enterprise
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment:
Windows Explorer
Modbus Device Importer
Resolution:
Power Monitoring Expert uses the config\translators folder for its custom device drivers. Only files in this folder will be used by the software. The config\templates folder is essentially a staging area for driver development until they are ready to be applied to the system. When drivers are created using the Modbus Device Importer, the program will default to the config\templates folder to save the .ion and .xml files (although the files can be saved in any location). When "Add Device Type" or "Update Device Type" is selected in the Modbus Device Importer, the driver files are then copied into the config\translators and are ready for use. There will now be two sets of the same driver files, one in the config\templates folder and the other in the config\translators.
At this point, it is possible to modify either set of files. If the files in the config\templates folder are opened in the Modbus Device Importer and modified, those changes will automatically be copied to the files in the config\translators folder upon selecting "Update Device Type".
Note: In Power Monitoring Expert 9.0, the Device Type Editor has been added as a replacement for the Modbus Device Importer. Using the DTE to modify drivers in the config\translators folder will result in a "file in use" error when attempting to install the driver. Therefore the files in the config\templates must be modified and any changes will then be applied to the config\translators files when the driver is installed.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: