{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the latest released version of the (MBX Driver Suite) Modbus Plus Driver?
MBX Driver Suite V9.0
Part# SWMXDS001

This driver is delivered with the following products:

416NHM21234
TSXCUSBMBP
416NHM30042A

Version 9.0  supports:
Windows 10
Windows 8
Windows 7 SP1
Windows Server 2016
Windows Server 2012
Windows Server 2008 R2 SP1

Schneider Electric Egypt and North East Africa