Search FAQs
The 'PRMMasterSetup.exe' version 1.1.4.0 installs DTM version 1.1.3.0
Issue
Unity shows the DTM version as 1.1.3.0 for the DTM that is installed using 'PRMMasterSetup.exe' version 1.1.4.0.
Product Line
TCSEGPA23F14F, M580, M340
Environment
TCSEGPA23F14F version 1.1.3.0
Resolution
After installing the Master DTM version 1.1.4.0, Unity shows the version of the DTM as 1.1.3.0.
![img1 img1](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009P4WuQAK&oid=00DA0000000abSm)
![img2 img2](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009P4WvQAK&oid=00DA0000000abSm)
![img3 img3](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009P4XfQAK&oid=00DA0000000abSm)
The installation window and the Properties Details tab for the setup is incorrectly labeld as 1.1.4.0. It should be 1.1.3.0.
Unity shows the DTM version as 1.1.3.0 for the DTM that is installed using 'PRMMasterSetup.exe' version 1.1.4.0.
Product Line
TCSEGPA23F14F, M580, M340
Environment
TCSEGPA23F14F version 1.1.3.0
Resolution
After installing the Master DTM version 1.1.4.0, Unity shows the version of the DTM as 1.1.3.0.
The installation window and the Properties Details tab for the setup is incorrectly labeld as 1.1.4.0. It should be 1.1.3.0.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: