{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you change the color of an object from the Toolchest in Vijeo Designer?
Issue:
Can you change the color of an object from the Toolchest in Vijeo Designer?

Product Line:
Vijeo Designer, Toolchest

Resolution:
No, you can not.  A work around would be to copy the object out of Vijeo Designer and paste it into a photo editing software (ex MS Paint). With the photo editing software, change the color of the object and save a new file for each of the different colors. Next, use a lamp object in Vijeo Designer that has the user defined category selected and browse the image file for ON and OFF.

Schneider Electric Egypt and North East Africa