{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for the Magelis XBTGT5430 HMI?
The Magelis XBTGT5430 is obsolete and has been replaced by the HMIDT542 + HMIG3U.

Migration Considerations:
- These new products are configured by the Vijeo Designer Software, version V6.2 SP1 minimum
- Vijeo Designer applications  are 100 % compatible.
- The cut-out is identical (*The new HMIGTU is comprised of two modules*)
- Screen resolution SVGA.
- The serial communication ports are identical  but COM1 Subd9 RS422/R232C becomes the COM2 and the COM2 RJ45 RS485 becomes the COM1
- Ethernet port with higher speed and with a second port
- Same certifications.
- Possible Extension Bus for Fieldbus modules ( Profibus , DeviceNet , CANopen )
- No support of SoMachine PLC functions
- Same auxiliary interface for speaker or alarm output
- Better Screen color TFT LED 16M and more resolution , More Flash Memory , addition mini-USB Device + Host/Device front USB ports  and use of SD card  slot.

Schneider Electric Egypt and North East Africa