Issue:
How do we determine what the maximum number of TCP/IP connections we can use on an HMI running the Vijeo Designer Runtime?
Product Line:
Vijeo Designer Runtime, Magelis (XBTGT, XBTGK, XBTGH, HMISTO, HMISTU, HMIGTO, HMIGTU)
Resolution:
The maximum number of TCP/IP connections depends on the model of the HMI used. For all non-iPC Magelis HMIs programmed with Vijeo Designer, the maximum number of TCP/IP connections is 48. In other words, you can add upto 48 TCP/IP equipments at the I/O Manager for models such as XBTGT, HMIGTO, HMISTO, HMIGTU, HMISTU, and HMIG3U.
For iPC models and HMIG5U, the limit is 80.
How do we determine what the maximum number of TCP/IP connections we can use on an HMI running the Vijeo Designer Runtime?
Product Line:
Vijeo Designer Runtime, Magelis (XBTGT, XBTGK, XBTGH, HMISTO, HMISTU, HMIGTO, HMIGTU)
Resolution:
The maximum number of TCP/IP connections depends on the model of the HMI used. For all non-iPC Magelis HMIs programmed with Vijeo Designer, the maximum number of TCP/IP connections is 48. In other words, you can add upto 48 TCP/IP equipments at the I/O Manager for models such as XBTGT, HMIGTO, HMISTO, HMIGTU, HMISTU, and HMIG3U.
For iPC models and HMIG5U, the limit is 80.
Released for:Schneider Electric Egypt and North East Africa