Search FAQs
What is the cable to connect a HMISTU to a Momentum PLC?
Issue:
Need to determine what cable is used to connect a HMISTU to a Momentum PLC?
Product Line:
Magelis (HMISTU/HMISTO/XBTGT/XBTGK/XBTGH/HMIGTO/HMIGTU)
Resolution:
The cable diagrams listed in the Modbus RTU driver manual of Vijeo Designer for this connection are:
XBTZG939 + XBTZ9711 for RS232 Communication
VW3A8306R10 For RS485 Communication.
NOTE: These cables do not apply for the 171CBU78090
Need to determine what cable is used to connect a HMISTU to a Momentum PLC?
Product Line:
Magelis (HMISTU/HMISTO/XBTGT/XBTGK/XBTGH/HMIGTO/HMIGTU)
Resolution:
The cable diagrams listed in the Modbus RTU driver manual of Vijeo Designer for this connection are:
XBTZG939 + XBTZ9711 for RS232 Communication
VW3A8306R10 For RS485 Communication.
NOTE: These cables do not apply for the 171CBU78090
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: