Search FAQs
What do the LED's on my Network Management Card mean?
Issue
The status and link LEDs (found on the left and right side of the ethernet port) on a Network Management Card give information on the current status of the NMC
Product Line
Network Management Card 2 / 3
![NMC front place NMC front place](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009P5dpQAC&oid=00DA0000000abSm)
![NMC3 faceplate](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CbfgpQAB&oid=00DA0000000abSmMAI)
The status LED (right side facing NMC2, left side facing NMC3) shows the following:
The Link LED (left side facing NMC2, right side facing NMC3) shows the following:
Network Management Card 4
![NMC front plate NMC front plate](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009P5dqQAC&oid=00DA0000000abSm)
The status LED (right side facing) shows the following:
The Link LED (left side facing) shows the following
The status and link LEDs (found on the left and right side of the ethernet port) on a Network Management Card give information on the current status of the NMC
Product Line
- Network Management Card 1 - AP9617, AP9618, AP9619
- Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH
- Network Management Card 4 – AP9644
Environment
- All firmware versions (unless otherwise noted)
- All serial numbers
Network Management Card 2 / 3
The status LED (right side facing NMC2, left side facing NMC3) shows the following:
LED Behavior | Meaning |
Off | The card is not receiving power or is in a boot up |
Solid Green | The card has valid IP settings |
Solid Orange | NMC2: Hardware Malfunction NMC3: In Bootmonitor mode or Hardware Malfunction |
Flashing Green | The card does not have valid IP settings |
Flashing Orange | The card is making BootP requests |
Alternating Green/Orange | Rapidly - The card is booting up |
Slowly - The card is making a DHCP request | |
Flickering Orange | NMC2: In Bootmonitor Mode. |
The Link LED (left side facing NMC2, right side facing NMC3) shows the following:
LED Behavior | Meaning |
Off | The card is not receiving power, does not have a connected network cable or the device (switch/hub) connected to the card is not active |
Solid Green | The card is on a network that communicates at 10Mbps |
Solid Orange | The card is on a network that communicates at 100Mbps |
Flashing Green | The card is receiving data packets at 10Mbps |
Flashing Orange | The card is receiving data packets at 100Mbps |
NMC3 Flashing Green | The card is receiving data packets at 1000Mbps |
Network Management Card 4
The status LED (right side facing) shows the following:
LED Behavior | Meaning |
Off | The card is not receiving power or is in a boot up |
Solid Green | The card has valid IP settings |
Solid Orange | The card does not have valid IP settings |
Alternating Green/Orange | Rapidly - The card is booting up |
Slowly - The card is making a DHCP request | |
Reset to factory default mode: | |
3 Short Orange | Password only reset* sequence activated *See the Security Handbook for information in relation to password only reset function. |
3 Short Green | NMC is resetting to factory defaults |
The Link LED (left side facing) shows the following
LED Behavior | Meaning |
Off | The card is not receiving power, does not have a connected network cable or the device (switch/hub) connected to the card is not active |
Solid Green | The card is on a network that communicates at 1 Gbps |
Solid Orange | The card is on a network that communicates at 10 or 100 Mbps |
Flashing Green | The card is receiving data packets at 1 Gbps |
Flashing Orange | The card is receiving data packets at 10 or 100Mbps |
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: