Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What cable is used to communicate via Modbus TCP/IP (USB Equipment) between the M340 to HMIGTO?
Issue:
Looking for assistance on how to connect the M340 PLC to a Magelis HMI in order to communicate over Modbus TCP/IP USB Equipment as defined in Vijeo Designer.

Product Line:
Vijeo Designer, Magelis HMI, M340 

Resolution:
The BMX-XCA-USBH018 is the cable to communicate by Modbus TCP/IP via USB between the M340 and the HMIGTO5310.

The mini-USB end plugs into the M340 and the standard USB end plugs into the HMIGTO

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: