{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference in the ATV212HD22N4 and ATV212HD22N4S?
Issue:
Differences between ATV212HD22N4 and ATV212HD22N4S

Product Line:
ATV212

Environment:
ATV212HD22N4   ATV212HD22N4S

Cause:
N/A

Resolution:
There was some extra margin in the next smaller frame size, so they made an ATV212HD22N4S for the U.S. market only.
It is smaller and for the same power as the original ATV212HD22N4, which is still used throughout the world.

It is the only frame size that had this margin, so the ATV212HD22N4S is the only S version and is available only in the U.S.

If you are running a standard motor, then the ATV212HD22N4S will save you space.
If you are running a heavy duty application, or using the Service Factor, you may want to use the larger ATV212HD22N4.


Schneider Electric Egypt and North East Africa