We have not implemented an alphanumeric identification today. If this is a strong request, we have to made a study. It is also necessary to keep in mind that the size of the display will limit the number of characters and the the freedom for names to be displayed is limited.
Released for:Schneider Electric Egypt and North East Africa
We have not implemented an alphanumeric identification today. If this is a strong request, we have to made a study. It is also necessary to keep in mind that the size of the display will limit the number of characters and the the freedom for names to be displayed is limited.