{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the max IP of enclosure in Tricast cast resin dry type transformers?
For indoor and outdoor applications we can provide up to IP 42 in Tricast dry type transformers. Furthermore, we can increase the ingress level up to IP55 for max power rating 3150 kVA with air conditioning application and 25MVA with water cool application.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.